Peak Power (dBm)

This is an analyzer sequence parameter which sets the peak power in dBm for the acquisition (information which is used by the Auto Set RF Level algorithm). If Auto Set RF Level (on the Meas Setup menu of the test set) is not set to On, this parameter is ignored.

There is no dropdown list for this field; it is necessary to enter a suitable value, or accept the default value of 0 dBm.